StyledCornerBuilderInteriorCurveTypes Enumeration¶
NXOpen.Features.StyledCornerBuilder.InteriorCurveTypes is an alias for NXOpen.Features.StyledCornerBuilderInteriorCurveTypes
-
class
NXOpen.Features.
StyledCornerBuilderInteriorCurveTypes
¶ Bases:
object
Intertior curve type
Enum Members
Enum Member Enum Member Description NotSet No interior curveIsoCurveU Iso u typeIsoCurveV Iso v typeIsoCurveUV Iso u and iso v type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-