StyledBlendBuilderStyledBlendTrimMethodType Enumeration

NXOpen.Features.StyledBlendBuilder.StyledBlendTrimMethodType is an alias for NXOpen.Features.StyledBlendBuilderStyledBlendTrimMethodType

class NXOpen.Features.StyledBlendBuilderStyledBlendTrimMethodType

Bases: object

The trim method types

Enum Members

Enum Member Enum Member Description
NoTrim
Non-trim
TrimAndAttach
Trim and attach
TrimInputWalls
Trim input walls
TrimInputBlends
Trim input blends
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.