StyledBlendBuilderStyledBlendShapeControlType Enumeration

NXOpen.Features.StyledBlendBuilder.StyledBlendShapeControlType is an alias for NXOpen.Features.StyledBlendBuilderStyledBlendShapeControlType

class NXOpen.Features.StyledBlendBuilderStyledBlendShapeControlType

Bases: object

The shape control types

Enum Members

Enum Member Enum Member Description
TangentCurve1
Tangent curve 1
TangentCurve2
Tangent curve 2
Depth
Depth control
Skew
Skew control
TangentMagnitude
Tangent magnitude control
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.