StudioXformBuilderExSurfaceDirectionType Enumeration

NXOpen.Features.StudioXformBuilderEx.SurfaceDirectionType is an alias for NXOpen.Features.StudioXformBuilderExSurfaceDirectionType

class NXOpen.Features.StudioXformBuilderExSurfaceDirectionType

Bases: object

Represents the U or V direction of a B-Surface

Enum Members

Enum Member Enum Member Description
U
U direction of a B-Surface
V
V direction of a B-Surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.