StudioXformBuilderExScalingCenterType Enumeration

NXOpen.Features.StudioXformBuilderEx.ScalingCenterType is an alias for NXOpen.Features.StudioXformBuilderExScalingCenterType

class NXOpen.Features.StudioXformBuilderExScalingCenterType

Bases: object

Represents the scaling center type

Enum Members

Enum Member Enum Member Description
Scaleaboutobjectcenter
Scale center at the object center
Scaleaboutselected
Scale center at the selected object
Scaleaboutpoint
Scale center at a point
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.