StudioXformBuilderExRotatingPivotType Enumeration

NXOpen.Features.StudioXformBuilderEx.RotatingPivotType is an alias for NXOpen.Features.StudioXformBuilderExRotatingPivotType

class NXOpen.Features.StudioXformBuilderExRotatingPivotType

Bases: object

Represents the rotating pivot type

Enum Members

Enum Member Enum Member Description
Rotateaboutobjectcenter
Rotate pivot at the object center
Rotateaboutselected
Rotate pivot at the selected object
Rotateaboutpoint
Rotate pivot at a point
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.