StudioXformBuilderExPrincipalScalingDirectionType Enumeration

NXOpen.Features.StudioXformBuilderEx.PrincipalScalingDirectionType is an alias for NXOpen.Features.StudioXformBuilderExPrincipalScalingDirectionType

class NXOpen.Features.StudioXformBuilderExPrincipalScalingDirectionType

Bases: object

Represents the principal scaling direction type

Enum Members

Enum Member Enum Member Description
X
Scale in X direction
Y
Scale in Y direction
Z
Scale in Z direction
YZ
Scale on Y-Z plane
XZ
Scale on X-Z plane
XY
Scale on X-Y plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.