StudioXformBuilderExPrincipalRotatingAxisType Enumeration

NXOpen.Features.StudioXformBuilderEx.PrincipalRotatingAxisType is an alias for NXOpen.Features.StudioXformBuilderExPrincipalRotatingAxisType

class NXOpen.Features.StudioXformBuilderExPrincipalRotatingAxisType

Bases: object

Represents the principal rotation axis type

Enum Members

Enum Member Enum Member Description
X
Rotate in X direction
Y
Rotate in Y direction
Z
Rotate in Z direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.