StudioXformBuilderExPlanarizeProjectionPlaneType Enumeration

NXOpen.Features.StudioXformBuilderEx.PlanarizeProjectionPlaneType is an alias for NXOpen.Features.StudioXformBuilderExPlanarizeProjectionPlaneType

class NXOpen.Features.StudioXformBuilderExPlanarizeProjectionPlaneType

Bases: object

Represents the planarize projection plane type

Enum Members

Enum Member Enum Member Description
YZ
On Y-Z plane when planarize
XZ
On X-Z plane when planarize
XY
On X-Y plane when planarize
Plane
On arbitrary plane when planarize
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.