StudioXformBuilderExInsertPoleType Enumeration

NXOpen.Features.StudioXformBuilderEx.InsertPoleType is an alias for NXOpen.Features.StudioXformBuilderExInsertPoleType

class NXOpen.Features.StudioXformBuilderExInsertPoleType

Bases: object

Represents the insert pole type

Enum Members

Enum Member Enum Member Description
Next
Insert pole next to the selected pole
Previous
Insert pole previous to the selected pole
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.