StudioXformBuilderExInsertKnotDirectionType Enumeration

NXOpen.Features.StudioXformBuilderEx.InsertKnotDirectionType is an alias for NXOpen.Features.StudioXformBuilderExInsertKnotDirectionType

class NXOpen.Features.StudioXformBuilderExInsertKnotDirectionType

Bases: object

Represents the insert knot direction type

Enum Members

Enum Member Enum Member Description
UDirection
Insert knot in U direction
VDirection
Insert knot in V direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.