StudioXformBuilderExExtrationMethodType Enumeration

NXOpen.Features.StudioXformBuilderEx.ExtrationMethodType is an alias for NXOpen.Features.StudioXformBuilderExExtrationMethodType

class NXOpen.Features.StudioXformBuilderExExtrationMethodType

Bases: object

B-surface extraction method

Enum Members

Enum Member Enum Member Description
Original
Extract original surface
MinimumBounded
Extract minimum bounded surface
FittoBoundary
Extract surface fitted to boundary of face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.