StudioXformBuilderExAdvancedMethodOptionType Enumeration

NXOpen.Features.StudioXformBuilderEx.AdvancedMethodOptionType is an alias for NXOpen.Features.StudioXformBuilderExAdvancedMethodOptionType

class NXOpen.Features.StudioXformBuilderExAdvancedMethodOptionType

Bases: object

Represents the advanced method option type

Enum Members

Enum Member Enum Member Description
Proportional
Proportional movement
LockRegion
Lock region
InsertKnot
Insert knot
AdvancedOff
No advanced methods
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.