StudioSurfaceBuilderTransitionOptions Enumeration

NXOpen.Features.StudioSurfaceBuilder.TransitionOptions is an alias for NXOpen.Features.StudioSurfaceBuilderTransitionOptions

class NXOpen.Features.StudioSurfaceBuilderTransitionOptions

Bases: object

the transition control options when using By Points alignment method

Enum Members

Enum Member Enum Member Description
NormalToEndSections
Normal to End Sections
NormalToAllSections
Normal to All Sections
Cubic
Cubic
LinearAndBlend
Linear and Blend
NoEndConstraint
No End Constraint
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.