StudioSplineBuilderExTypes Enumeration

NXOpen.Features.StudioSplineBuilderEx.Types is an alias for NXOpen.Features.StudioSplineBuilderExTypes

class NXOpen.Features.StudioSplineBuilderExTypes

Bases: object

Spline methods.

Enum Members

Enum Member Enum Member Description
ThroughPoints
Spline through points
ByPoles
Spline by poles
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.