StudioSplineBuilderExMatchKnotsTypes Enumeration¶
NXOpen.Features.StudioSplineBuilderEx.MatchKnotsTypes is an alias for NXOpen.Features.StudioSplineBuilderExMatchKnotsTypes
-
class
NXOpen.Features.
StudioSplineBuilderExMatchKnotsTypes
¶ Bases:
object
Options for creating knots at the defining points in case of through point spline
Enum Members
Enum Member Enum Member Description NotSet No knot matchingCubic Match knots for cubic non-periodic splineGeneral Match knots for general spline-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-