StudioSplineBuilderExInputCurveOptions Enumeration

NXOpen.Features.StudioSplineBuilderEx.InputCurveOptions is an alias for NXOpen.Features.StudioSplineBuilderExInputCurveOptions

class NXOpen.Features.StudioSplineBuilderExInputCurveOptions

Bases: object

Options of the actions to be taken on an input non-parametric spline after its editing is done.

These options are used only while trying to make non-parametric spline a feature.

Enum Members

Enum Member Enum Member Description
Keep
Keep original curve
Hide
Hide original curve
Delete
Delete original curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.