StudioSplineBuilderExDrawingPlaneOptions Enumeration

NXOpen.Features.StudioSplineBuilderEx.DrawingPlaneOptions is an alias for NXOpen.Features.StudioSplineBuilderExDrawingPlaneOptions

class NXOpen.Features.StudioSplineBuilderExDrawingPlaneOptions

Bases: object

Drawing plane options

Enum Members

Enum Member Enum Member Description
View
View plane
XY
XY plane
YZ
YZ plane
XZ
XZ plane
General
General plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.