StudioSplineBuilderCurveOption Enumeration

NXOpen.Features.StudioSplineBuilder.CurveOption is an alias for NXOpen.Features.StudioSplineBuilderCurveOption

class NXOpen.Features.StudioSplineBuilderCurveOption

Bases: object

Options of the actions to be taken on an input non-parametric spline after its editing is done.

These options are used only while trying to make non-parametric spline a feature.

Enum Members

Enum Member Enum Member Description
Retain
Retain input curve
Blank
Blank input curve
Delete
Delete input curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.