StepBuilderStepTypes Enumeration

NXOpen.Features.StepBuilder.StepTypes is an alias for NXOpen.Features.StepBuilderStepTypes

class NXOpen.Features.StepBuilderStepTypes

Bases: object

Represents the step feature type

Enum Members

Enum Member Enum Member Description
End
Adds a step from a boundary to the edge of a face.
Middle
Adds a step between two boundary curves
Chamfer Adds a step at the edge of a face similar to a chamfer
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.