StepBuilderReferenceBoundaryTypes Enumeration

NXOpen.Features.StepBuilder.ReferenceBoundaryTypes is an alias for NXOpen.Features.StepBuilderReferenceBoundaryTypes

class NXOpen.Features.StepBuilderReferenceBoundaryTypes

Bases: object

Represents selected type as reference boundary object

Enum Members

Enum Member Enum Member Description
Face
Select faces as reference boundary object
DatumPlane
Select datum plane as reference boundary object
Curve
Select section curves as reference boundary object
Edge
Select edges as reference boundary object
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.