SpineCurveBuilder Class¶
-
class
NXOpen.Features.
SpineCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
Features.SpineCurve
builderTo create a new instance of this class, use
NXOpen.Features.FreeformCurveCollection.CreateSpineCurveBuilder()
Default values.
Property Value Associative 0 Closed 0 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ArcSegmentsType | Returns or sets the option indicating type of shape |
Associative | Returns or sets the flag indicating if an associative Spine Curve (Feature) should be created. |
Closed | Returns or sets the flag indicating if a closed curve should be created if possible. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseStartDirection | Returns or sets the flag indicating if starting direction of the curve should be opposite to the first plane normal. |
StartPoint | Returns or sets the start point |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ThroughPlanesList | Returns the plane list containing the through planes. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
Evaluate | Evaluates the curve |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SpineCurveBuilderArcSegmentsTypes Enumeration | This enum represents the arc segments types |
Property Detail¶
ArcSegmentsType¶
-
SpineCurveBuilder.
ArcSegmentsType
¶ Returns or sets the option indicating type of shape
-------------------------------------
Getter Method
Signature
ArcSegmentsType()
Returns: Return type: NXOpen.Features.SpineCurveBuilderArcSegmentsTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcSegmentsType(curveOption)
Parameters: curveOption ( NXOpen.Features.SpineCurveBuilderArcSegmentsTypes
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Associative¶
-
SpineCurveBuilder.
Associative
¶ Returns or sets the flag indicating if an associative Spine Curve (Feature) should be created.
-------------------------------------
Getter Method
Signature
Associative()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative(associative)
Parameters: associative (bool) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Closed¶
-
SpineCurveBuilder.
Closed
¶ Returns or sets the flag indicating if a closed curve should be created if possible.
-------------------------------------
Getter Method
Signature
Closed()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Closed(closed)
Parameters: closed (bool) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ReverseStartDirection¶
-
SpineCurveBuilder.
ReverseStartDirection
¶ Returns or sets the flag indicating if starting direction of the curve should be opposite to the first plane normal.
-------------------------------------
Getter Method
Signature
ReverseStartDirection()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseStartDirection(direction)
Parameters: direction (bool) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
StartPoint¶
-
SpineCurveBuilder.
StartPoint
¶ Returns or sets the start point
-------------------------------------
Getter Method
Signature
StartPoint()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPoint(startPoint)
Parameters: startPoint ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ThroughPlanesList¶
-
SpineCurveBuilder.
ThroughPlanesList
¶ Returns the plane list containing the through planes.
-------------------------------------
Getter Method
Signature
ThroughPlanesList()
Returns: Return type: NXOpen.GeometricUtilities.SpinePlaneBuilderList
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Evaluate¶
-
SpineCurveBuilder.
Evaluate
¶ Evaluates the curve
Signature
Evaluate()
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
SpineCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.