SmoothSplineBuilderTypes Enumeration

NXOpen.Features.SmoothSplineBuilder.Types is an alias for NXOpen.Features.SmoothSplineBuilderTypes

class NXOpen.Features.SmoothSplineBuilderTypes

Bases: object

This enum represents the Smoothing Type option

Enum Members

Enum Member Enum Member Description
Curvature
Curvature
CurvatureVariation
Curvature Variation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.