SketchConversionStatusType Enumeration

NXOpen.Features.SketchConversionStatus.Type is an alias for NXOpen.Features.SketchConversionStatusType

class NXOpen.Features.SketchConversionStatusType

Bases: object

Status of conversion - Success, Failure or Partial-Success

Enum Members

Enum Member Enum Member Description
Success
Convert to sketch successful
Failure
Convert to sketch failed
PartialSuccess
Convert to sketch succeeded with reason/issues
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.