SilhouetteFlangeBuilderOutputSurfaceOptions Enumeration

NXOpen.Features.SilhouetteFlangeBuilder.OutputSurfaceOptions is an alias for NXOpen.Features.SilhouetteFlangeBuilderOutputSurfaceOptions

class NXOpen.Features.SilhouetteFlangeBuilderOutputSurfaceOptions

Bases: object

Output surface options

Enum Members

Enum Member Enum Member Description
BlendFlange
Output blend and flange surfaces
PipeOnly
Output pipe
FlangeOnly
Output flange surface
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.