WeightAndCGBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
WeightAndCGBuilder
¶ Bases:
NXOpen.Builder
Represents the class Features.
ShipDesign.WeightAndCGBuilder which is used to calculate the weight and cg information.
To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateWeightAndCgBuilder()
Default values.
Property Value SelectionMethod Volume New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
SelectionMethod | Returns or sets the selection method. |
Tag | Returns the Tag for this object. |
VolumeBody | Returns the selected volume body. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetFrameParts | Sets the selected frame parts. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
WeightAndCGBuilderSelectionMethods Enumeration | Settings to indicate how the objects are selected. |
Property Detail¶
SelectionMethod¶
-
WeightAndCGBuilder.
SelectionMethod
¶ Returns or sets the selection method.
-------------------------------------
Getter Method
Signature
SelectionMethod()
Returns: Return type: NXOpen.Features.ShipDesign.WeightAndCGBuilderSelectionMethods
New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
-------------------------------------
Setter Method
Signature
SelectionMethod(enumSelectionType)
Parameters: enumSelectionType ( NXOpen.Features.ShipDesign.WeightAndCGBuilderSelectionMethods
) –New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
VolumeBody¶
-
WeightAndCGBuilder.
VolumeBody
¶ Returns the selected volume body.
-------------------------------------
Getter Method
Signature
VolumeBody()
Returns: Return type: NXOpen.SelectBody
New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Method Detail¶
SetFrameParts¶
-
WeightAndCGBuilder.
SetFrameParts
¶ Sets the selected frame parts.
Signature
SetFrameParts(nPartCount)
Parameters: nPartCount (int) – Returns: ship basic design structure component. Return type: NXOpen.Part
New in version NX10.0.0.
License requirements: nx_ship_basic (“Ship Basic Design”)
Validate¶
-
WeightAndCGBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.