UpdateShipLibraryBuilderShipLibOptionType Enumeration¶
NXOpen.Features.ShipDesign.UpdateShipLibraryBuilder.ShipLibOptionType is an alias for NXOpen.Features.ShipDesign.UpdateShipLibraryBuilderShipLibOptionType
-
class
NXOpen.Features.ShipDesign.
UpdateShipLibraryBuilderShipLibOptionType
¶ Bases:
object
Ship Library Types Note the weld along edge option is no longer used in NX7.
5, and will be removed in NX8.
Enum Members
Enum Member Enum Member Description Profile Belt Cutout Endcut Support SupportCap WeldOnEdge Bracket WeldAlongEdge obsolete in NX7.5-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-