TransitionBuilderTransitionTypes Enumeration¶
NXOpen.Features.ShipDesign.TransitionBuilder.TransitionTypes is an alias for NXOpen.Features.ShipDesign.TransitionBuilderTransitionTypes
-
class
NXOpen.Features.ShipDesign.
TransitionBuilderTransitionTypes
¶ Bases:
object
Transition Type.
Section type means the basic design elements in speicified ship section will be transitioned. Frame type means specified basic design elements will be transitioned.
Enum Members
Enum Member Enum Member Description Section Frame -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-