ThicknessDirectionBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ThicknessDirectionBuilder
¶ Bases:
NXOpen.Builder
This class allows you to define the thickness direction for plate system features in Ship Basic Design and and for grid planes in Ship Concept Design.
This class is sub-object of another builder, and cannot be directly instantiated.
Default values.
Property Value ThicknessDirection FwdPortInUp ThicknessDirectionOnReference FwdPortInUp New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ThicknessDirection | Returns or sets the direction in which to apply the thickness. |
ThicknessDirectionOnReference | Returns or sets the direction in which to apply the thickness when the mold face or grid plane is located on a midship reference. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ThicknessDirectionBuilderThicknessDirectionType Enumeration | Settings used to indicate the direction of thickness from the mold face or grid plane. |
Property Detail¶
ThicknessDirection¶
-
ThicknessDirectionBuilder.
ThicknessDirection
¶ Returns or sets the direction in which to apply the thickness.
-------------------------------------
Getter Method
Signature
ThicknessDirection()
Returns: Return type: NXOpen.Features.ShipDesign.ThicknessDirectionBuilderThicknessDirectionType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessDirection(thicknessDirection)
Parameters: thicknessDirection ( NXOpen.Features.ShipDesign.ThicknessDirectionBuilderThicknessDirectionType
) –New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
ThicknessDirectionOnReference¶
-
ThicknessDirectionBuilder.
ThicknessDirectionOnReference
¶ Returns or sets the direction in which to apply the thickness when the mold face or grid plane is located on a midship reference.
-------------------------------------
Getter Method
Signature
ThicknessDirectionOnReference()
Returns: Return type: NXOpen.Features.ShipDesign.ThicknessDirectionBuilderThicknessDirectionType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThicknessDirectionOnReference(thicknessDirectionOnReference)
Parameters: thicknessDirectionOnReference ( NXOpen.Features.ShipDesign.ThicknessDirectionBuilderThicknessDirectionType
) –New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”) OR nx_ship_basic (“Ship Basic Design”) OR nx_ship_detail (“Ship Detail Design”)
Method Detail¶
Validate¶
-
ThicknessDirectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.