StiffenerLimitBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
StiffenerLimitBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class defines the path limit method used by a Stiffener or Edge Reinforcement feature.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
LimitGeometry | Returns the limiting geometry |
LimitMethod | Returns or sets the limit method |
LimitValue | Returns the fixed limiting value |
SquareCutClearance | Returns the limit clearance value |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StiffenerLimitBuilderLimitType Enumeration | Path limiting method |
Property Detail¶
LimitGeometry¶
-
StiffenerLimitBuilder.
LimitGeometry
¶ Returns the limiting geometry
-------------------------------------
Getter Method
Signature
LimitGeometry()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: None.
LimitMethod¶
-
StiffenerLimitBuilder.
LimitMethod
¶ Returns or sets the limit method
-------------------------------------
Getter Method
Signature
LimitMethod()
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerLimitBuilderLimitType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitMethod(limitMethod)
Parameters: limitMethod ( NXOpen.Features.ShipDesign.StiffenerLimitBuilderLimitType
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
LimitValue¶
-
StiffenerLimitBuilder.
LimitValue
¶ Returns the fixed limiting value
-------------------------------------
Getter Method
Signature
LimitValue()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SquareCutClearance¶
-
StiffenerLimitBuilder.
SquareCutClearance
¶ Returns the limit clearance value
-------------------------------------
Getter Method
Signature
SquareCutClearance()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
StiffenerLimitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.