StiffenerBySupportPathBuilderMethod Enumeration¶
NXOpen.Features.ShipDesign.StiffenerBySupportPathBuilder.Method is an alias for NXOpen.Features.ShipDesign.StiffenerBySupportPathBuilderMethod
-
class
NXOpen.Features.ShipDesign.
StiffenerBySupportPathBuilderMethod
¶ Bases:
object
Type of Stiffener by Support Method
Enum Members
Enum Member Enum Member Description AlignedBoundary Aligned BoundaryAlignedLength Aligned LengthBoundToBound Bound to BoundParallelToLine Parallel to LineHorizontal HorizontalVertical VerticalNormalToCurve Normal to CurveThroughPoint Through Point-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-