StiffenerBuilderEdgeReinforcementAlignmentMethod Enumeration¶
NXOpen.Features.ShipDesign.StiffenerBuilder.EdgeReinforcementAlignmentMethod is an alias for NXOpen.Features.ShipDesign.StiffenerBuilderEdgeReinforcementAlignmentMethod
-
class
NXOpen.Features.ShipDesign.
StiffenerBuilderEdgeReinforcementAlignmentMethod
¶ Bases:
object
the edge reinforcement alignment method
Enum Members
Enum Member Enum Member Description Center Center the Edge Reinforcement on the selected edgeGuideEdge Place the end of the Edge Reinforcement on the selected edgeOppositeGuide Place the end of the Edge Reinforcement on the edge opposite the selected edge-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-