StiffenerBuilderAttachmentOption Enumeration¶
NXOpen.Features.ShipDesign.StiffenerBuilder.AttachmentOption is an alias for NXOpen.Features.ShipDesign.StiffenerBuilderAttachmentOption
-
class
NXOpen.Features.ShipDesign.
StiffenerBuilderAttachmentOption
¶ Bases:
object
The stiffener attachment plate option
Enum Members
Enum Member Enum Member Description Inferred Infer the plate on which to attach the stiffenerOverride Use the selected attachment plate on which to attach the stiffener-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-