SteelSupportBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
SteelSupportBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.SteelSupport
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateSteelSupportBuilder()
Default values.
Property Value AngularDim.Value 0 EndCapThickness.Value 0 (millimeters part), 0 (inches part) EndOffset.Value 0 (millimeters part), 0 (inches part) Line1Offset.Value 0 (millimeters part), 0 (inches part) Line2Offset.Value 0 (millimeters part), 0 (inches part) PlacementMethod TwoPlanesandLines StartCapThickness.Value 0 (millimeters part), 0 (inches part) StartOffset.Value 0 (millimeters part), 0 (inches part) SupportCapOptions None New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AngularDim | Returns the angular dimension used to rotate the support feature. |
AttributeMaterial | Returns or sets the attribute material |
AttributeName | Returns or sets the name attribute value |
CoordSystem | Returns or sets the coord system (only used with SpecifyCsys creation method) |
EndCapSize | Returns or sets the end cap size. |
EndCapThickness | Returns the end cap thickness |
EndCapType | Returns or sets the end cap type. |
EndOffset | Returns the offset used to determine where the support ends (used with SpecifyLine and SpecifyCsys creation methods) |
EndPlane | Returns or sets the end plane (only used with TwoPlanesandLines creation method) |
KeepCoordSystem | Returns or sets whether or not we should keep the selected csys on apply (only used with SpecifyCsys creation method) |
KeepEndPlane | Returns or sets whether or not we should keep the selected end plane on apply (only used with TwoPlanesandLines creation method) |
KeepReverseEndOffset | Returns or sets the keep previous reverse setting on apply (used with SpecifyLine and SpecifyCsys creation methods) |
KeepReverseLine1Offset | Returns or sets the keep previous reverse setting on apply (only used with TwoPlanesandLines creation method) |
KeepReverseLine2Offset | Returns or sets the keep previous reverse setting on apply (only used with TwoPlanesandLines creation method) |
KeepReverseStartOffset | Returns or sets the keep previous reverse setting on apply (used with SpecifyLine and SpecifyCsys creation methods) |
KeepSelectGuideCurve | Returns or sets whether or not we should keep the selected guide curve on apply (only used with SpecifyLine creation method) |
KeepSelectLine1 | Returns or sets whether or not we should keep the selected first line on apply (only used with TwoPlanesandLines creation method) |
KeepSelectLine2 | Returns or sets whether or not we should keep the selected second line on apply (only used with TwoPlanesandLines creation method) |
KeepSelectOrientationLine | Returns or sets whether or not we should keep the selected orientation line on apply (only used with SpecifyLine creation method) |
KeepStartPlane | Returns or sets whether or not we should keep the selected start plane on apply (only used with TwoPlanesandLines creation method) |
Line1Offset | Returns the first line offset (only used with TwoPlanesandLines creation method) |
Line2Offset | Returns the second line offset (only used with TwoPlanesandLines creation method) |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlacementMethod | Returns or sets the placement method used to create the feature |
ReverseEndOffset | Returns or sets the reverse end offset (used with SpecifyLine and SpecifyCsys creation methods) |
ReverseLine1Offset | Returns or sets the reverse first line offset (only used with TwoPlanesandLines creation method) |
ReverseLine2Offset | Returns or sets the reverse second line offset (only used with TwoPlanesandLines creation method) |
ReverseStartOffset | Returns or sets the reverse start offset (used with SpecifyLine and SpecifyCsys creation methods) |
SelectGuideCurve | Returns the select guide curve (only used with SpecifyLine creation method) |
SelectLine1 | Returns the first line (only used with TwoPlanesandLines creation method) |
SelectLine2 | Returns the second line (only used with TwoPlanesandLines creation method) |
SelectOrientationLine | Returns the orientation line (only used with SpecifyLine creation method) |
StartCapSize | Returns or sets the start cap size. |
StartCapThickness | Returns the start cap thickness |
StartCapType | Returns or sets the start cap type. |
StartOffset | Returns the offset used to determine where the support starts (used with SpecifyLine and SpecifyCsys creation methods) |
StartPlane | Returns or sets the start plane (only used with TwoPlanesandLines creation method) |
SupportCapOptions | Returns or sets the support cap options |
SupportSize | Returns or sets the support size. |
SupportType | Returns or sets the support type. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAvailableAttributeMaterials | Returns the list of available material attributes @return Array of available attribute materials. |
GetAvailableAttributeNames | Returns the list of available name attributes @return Array of available attribute names. |
GetAvailableCapTypes | The list of available start and end cap types. |
GetAvailableEndCapSizes | The list of available end cap sizes. |
GetAvailableStartCapSizes | The list of available start cap sizes. |
GetAvailableSupportSizes | The list of available sizes. |
GetAvailableSupportTypes | The list of available support types. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SteelSupportBuilderCapOptions Enumeration | Does this feature have end caps, and if so what kind? |
SteelSupportBuilderCreationMethod Enumeration | Method used to create the support feature |
Property Detail¶
AngularDim¶
-
SteelSupportBuilder.
AngularDim
¶ Returns the angular dimension used to rotate the support feature.
-------------------------------------
Getter Method
Signature
AngularDim()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
AttributeMaterial¶
-
SteelSupportBuilder.
AttributeMaterial
¶ Returns or sets the attribute material
-------------------------------------
Getter Method
Signature
AttributeMaterial()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttributeMaterial(attributeMaterial)
Parameters: attributeMaterial (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
AttributeName¶
-
SteelSupportBuilder.
AttributeName
¶ Returns or sets the name attribute value
-------------------------------------
Getter Method
Signature
AttributeName()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttributeName(attributeName)
Parameters: attributeName (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
CoordSystem¶
-
SteelSupportBuilder.
CoordSystem
¶ Returns or sets the coord system (only used with “SpecifyCsys” creation method)
-------------------------------------
Getter Method
Signature
CoordSystem()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordSystem(coordSystem)
Parameters: coordSystem ( NXOpen.CoordinateSystem
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
EndCapSize¶
-
SteelSupportBuilder.
EndCapSize
¶ Returns or sets the end cap size.
Determines the cross section of the support cap.
-------------------------------------
Getter Method
Signature
EndCapSize()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCapSize(endCapSize)
Parameters: endCapSize (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
EndCapThickness¶
-
SteelSupportBuilder.
EndCapThickness
¶ Returns the end cap thickness
-------------------------------------
Getter Method
Signature
EndCapThickness()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
EndCapType¶
-
SteelSupportBuilder.
EndCapType
¶ Returns or sets the end cap type.
Determines the cross section of the support cap.
-------------------------------------
Getter Method
Signature
EndCapType()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCapType(endCapType)
Parameters: endCapType (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
EndOffset¶
-
SteelSupportBuilder.
EndOffset
¶ Returns the offset used to determine where the support ends (used with “SpecifyLine” and “SpecifyCsys” creation methods)
-------------------------------------
Getter Method
Signature
EndOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
EndPlane¶
-
SteelSupportBuilder.
EndPlane
¶ Returns or sets the end plane (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
EndPlane()
Returns: Return type: NXOpen.Plane
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPlane(endPlane)
Parameters: endPlane ( NXOpen.Plane
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepCoordSystem¶
-
SteelSupportBuilder.
KeepCoordSystem
¶ Returns or sets whether or not we should keep the selected csys on apply (only used with “SpecifyCsys” creation method)
-------------------------------------
Getter Method
Signature
KeepCoordSystem()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepCoordSystem(keepCoordSystem)
Parameters: keepCoordSystem (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepEndPlane¶
-
SteelSupportBuilder.
KeepEndPlane
¶ Returns or sets whether or not we should keep the selected end plane on apply (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
KeepEndPlane()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepEndPlane(keepEndPlane)
Parameters: keepEndPlane (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepReverseEndOffset¶
-
SteelSupportBuilder.
KeepReverseEndOffset
¶ Returns or sets the keep previous reverse setting on apply (used with “SpecifyLine” and “SpecifyCsys” creation methods)
-------------------------------------
Getter Method
Signature
KeepReverseEndOffset()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepReverseEndOffset(keepReverseEndOffset)
Parameters: keepReverseEndOffset (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepReverseLine1Offset¶
-
SteelSupportBuilder.
KeepReverseLine1Offset
¶ Returns or sets the keep previous reverse setting on apply (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
KeepReverseLine1Offset()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepReverseLine1Offset(keepReverseLine1Offset)
Parameters: keepReverseLine1Offset (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepReverseLine2Offset¶
-
SteelSupportBuilder.
KeepReverseLine2Offset
¶ Returns or sets the keep previous reverse setting on apply (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
KeepReverseLine2Offset()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepReverseLine2Offset(keepReverseLine2Offset)
Parameters: keepReverseLine2Offset (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepReverseStartOffset¶
-
SteelSupportBuilder.
KeepReverseStartOffset
¶ Returns or sets the keep previous reverse setting on apply (used with “SpecifyLine” and “SpecifyCsys” creation methods)
-------------------------------------
Getter Method
Signature
KeepReverseStartOffset()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepReverseStartOffset(keepReverseStartOffset)
Parameters: keepReverseStartOffset (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepSelectGuideCurve¶
-
SteelSupportBuilder.
KeepSelectGuideCurve
¶ Returns or sets whether or not we should keep the selected guide curve on apply (only used with “SpecifyLine” creation method)
-------------------------------------
Getter Method
Signature
KeepSelectGuideCurve()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepSelectGuideCurve(keepSelectGuideCurve)
Parameters: keepSelectGuideCurve (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepSelectLine1¶
-
SteelSupportBuilder.
KeepSelectLine1
¶ Returns or sets whether or not we should keep the selected first line on apply (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
KeepSelectLine1()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepSelectLine1(keepSelectLine1)
Parameters: keepSelectLine1 (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepSelectLine2¶
-
SteelSupportBuilder.
KeepSelectLine2
¶ Returns or sets whether or not we should keep the selected second line on apply (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
KeepSelectLine2()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepSelectLine2(keepSelectLine2)
Parameters: keepSelectLine2 (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepSelectOrientationLine¶
-
SteelSupportBuilder.
KeepSelectOrientationLine
¶ Returns or sets whether or not we should keep the selected orientation line on apply (only used with “SpecifyLine” creation method)
-------------------------------------
Getter Method
Signature
KeepSelectOrientationLine()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepSelectOrientationLine(keepSelectOrientationLine)
Parameters: keepSelectOrientationLine (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepStartPlane¶
-
SteelSupportBuilder.
KeepStartPlane
¶ Returns or sets whether or not we should keep the selected start plane on apply (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
KeepStartPlane()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepStartPlane(keepStartPlane)
Parameters: keepStartPlane (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
Line1Offset¶
-
SteelSupportBuilder.
Line1Offset
¶ Returns the first line offset (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
Line1Offset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Line2Offset¶
-
SteelSupportBuilder.
Line2Offset
¶ Returns the second line offset (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
Line2Offset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
PlacementMethod¶
-
SteelSupportBuilder.
PlacementMethod
¶ Returns or sets the placement method used to create the feature
-------------------------------------
Getter Method
Signature
PlacementMethod()
Returns: Return type: NXOpen.Features.ShipDesign.SteelSupportBuilderCreationMethod
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlacementMethod(placementMethod)
Parameters: placementMethod ( NXOpen.Features.ShipDesign.SteelSupportBuilderCreationMethod
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
ReverseEndOffset¶
-
SteelSupportBuilder.
ReverseEndOffset
¶ Returns or sets the reverse end offset (used with “SpecifyLine” and “SpecifyCsys” creation methods)
-------------------------------------
Getter Method
Signature
ReverseEndOffset()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseEndOffset(reverseEndOffset)
Parameters: reverseEndOffset (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
ReverseLine1Offset¶
-
SteelSupportBuilder.
ReverseLine1Offset
¶ Returns or sets the reverse first line offset (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
ReverseLine1Offset()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseLine1Offset(reverseLine1Offset)
Parameters: reverseLine1Offset (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
ReverseLine2Offset¶
-
SteelSupportBuilder.
ReverseLine2Offset
¶ Returns or sets the reverse second line offset (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
ReverseLine2Offset()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseLine2Offset(reverseLine2Offset)
Parameters: reverseLine2Offset (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
ReverseStartOffset¶
-
SteelSupportBuilder.
ReverseStartOffset
¶ Returns or sets the reverse start offset (used with “SpecifyLine” and “SpecifyCsys” creation methods)
-------------------------------------
Getter Method
Signature
ReverseStartOffset()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseStartOffset(reverseStartOffset)
Parameters: reverseStartOffset (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
SelectGuideCurve¶
-
SteelSupportBuilder.
SelectGuideCurve
¶ Returns the select guide curve (only used with “SpecifyLine” creation method)
-------------------------------------
Getter Method
Signature
SelectGuideCurve()
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX7.5.0.
License requirements: None.
SelectLine1¶
-
SteelSupportBuilder.
SelectLine1
¶ Returns the first line (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
SelectLine1()
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX7.5.0.
License requirements: None.
SelectLine2¶
-
SteelSupportBuilder.
SelectLine2
¶ Returns the second line (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
SelectLine2()
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX7.5.0.
License requirements: None.
SelectOrientationLine¶
-
SteelSupportBuilder.
SelectOrientationLine
¶ Returns the orientation line (only used with “SpecifyLine” creation method)
-------------------------------------
Getter Method
Signature
SelectOrientationLine()
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX7.5.0.
License requirements: None.
StartCapSize¶
-
SteelSupportBuilder.
StartCapSize
¶ Returns or sets the start cap size.
Determines the cross section of the support cap.
-------------------------------------
Getter Method
Signature
StartCapSize()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartCapSize(startCapSize)
Parameters: startCapSize (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
StartCapThickness¶
-
SteelSupportBuilder.
StartCapThickness
¶ Returns the start cap thickness
-------------------------------------
Getter Method
Signature
StartCapThickness()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
StartCapType¶
-
SteelSupportBuilder.
StartCapType
¶ Returns or sets the start cap type.
Determines the cross section of the support cap.
-------------------------------------
Getter Method
Signature
StartCapType()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartCapType(startCapType)
Parameters: startCapType (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
StartOffset¶
-
SteelSupportBuilder.
StartOffset
¶ Returns the offset used to determine where the support starts (used with “SpecifyLine” and “SpecifyCsys” creation methods)
-------------------------------------
Getter Method
Signature
StartOffset()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
StartPlane¶
-
SteelSupportBuilder.
StartPlane
¶ Returns or sets the start plane (only used with “TwoPlanesandLines” creation method)
-------------------------------------
Getter Method
Signature
StartPlane()
Returns: Return type: NXOpen.Plane
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPlane(startPlane)
Parameters: startPlane ( NXOpen.Plane
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
SupportCapOptions¶
-
SteelSupportBuilder.
SupportCapOptions
¶ Returns or sets the support cap options
-------------------------------------
Getter Method
Signature
SupportCapOptions()
Returns: Return type: NXOpen.Features.ShipDesign.SteelSupportBuilderCapOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SupportCapOptions(supportCapOptions)
Parameters: supportCapOptions ( NXOpen.Features.ShipDesign.SteelSupportBuilderCapOptions
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
SupportSize¶
-
SteelSupportBuilder.
SupportSize
¶ Returns or sets the support size.
Determines the cross section of the support.
-------------------------------------
Getter Method
Signature
SupportSize()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SupportSize(supportSize)
Parameters: supportSize (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
SupportType¶
-
SteelSupportBuilder.
SupportType
¶ Returns or sets the support type.
Determines the cross section of the support.
-------------------------------------
Getter Method
Signature
SupportType()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SupportType(supportType)
Parameters: supportType (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
Method Detail¶
GetAvailableAttributeMaterials¶
-
SteelSupportBuilder.
GetAvailableAttributeMaterials
¶ Returns the list of available material attributes
Signature
GetAvailableAttributeMaterials()
Returns: Array of available attribute materials. These materials are specified in the customer defaults file. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableAttributeNames¶
-
SteelSupportBuilder.
GetAvailableAttributeNames
¶ Returns the list of available name attributes
Signature
GetAvailableAttributeNames()
Returns: Array of available attribute names. These names are specified in the customer defaults file. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableCapTypes¶
-
SteelSupportBuilder.
GetAvailableCapTypes
¶ The list of available start and end cap types.
Signature
GetAvailableCapTypes()
Returns: Array of available cap types. These names are specified by a special sketch naming convention for sketches loaded in the support cap library. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableEndCapSizes¶
-
SteelSupportBuilder.
GetAvailableEndCapSizes
¶ The list of available end cap sizes.
The available end cap sizes will change everytime the end cap type changes.
Signature
GetAvailableEndCapSizes()
Returns: Array of available end cap sizes. These names are specified by a special sketch naming convention for sketches loaded in the support cap library. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableStartCapSizes¶
-
SteelSupportBuilder.
GetAvailableStartCapSizes
¶ The list of available start cap sizes.
The available start cap sizes will change everytime the start cap type changes.
Signature
GetAvailableStartCapSizes()
Returns: Array of available start cap sizes. These names are specified by a special sketch naming convention for sketches loaded in the support cap library. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableSupportSizes¶
-
SteelSupportBuilder.
GetAvailableSupportSizes
¶ The list of available sizes.
The available sizes will change everytime the support type changes.
Signature
GetAvailableSupportSizes()
Returns: Array of available sizes. These names are specified by a special sketch naming convention for sketches loaded in the support library. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableSupportTypes¶
-
SteelSupportBuilder.
GetAvailableSupportTypes
¶ The list of available support types.
Signature
GetAvailableSupportTypes()
Returns: Array of available types. These names are specified by a special sketch naming convention for sketches loaded in the support library. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
Validate¶
-
SteelSupportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.