SteelInsulationBoundaryBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
SteelInsulationBoundaryBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a Steel Insulation Boundary builder.
The steel insulation boundary is used to collect boundary information that includes how much to offset the insulation from the selected boundary. The builder is used when creating/editing a
NXOpen.Features.ShipDesign.SteelInsulation
feature.To create a new instance of this class, use
NXOpen.Features.ShipDesign.SteelInsulationBuilder.CreateSteelInsulationBoundary()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Boundaries | Returns the face or edges that will be used to bound the insulation body. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateOffsetExpressions | Create offset expressions for each boundary. |
GetOffsetExpressions | Get offset expressions for each boundary. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Boundaries¶
-
SteelInsulationBoundaryBuilder.
Boundaries
¶ Returns the face or edges that will be used to bound the insulation body.
-------------------------------------
Getter Method
Signature
Boundaries()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
Method Detail¶
CreateOffsetExpressions¶
-
SteelInsulationBoundaryBuilder.
CreateOffsetExpressions
¶ Create offset expressions for each boundary.
Signature
CreateOffsetExpressions()
New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
GetOffsetExpressions¶
-
SteelInsulationBoundaryBuilder.
GetOffsetExpressions
¶ Get offset expressions for each boundary.
Signature
GetOffsetExpressions()
Returns: boundary Offset Expressions. Return type: list of NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Validate¶
-
SteelInsulationBoundaryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.