StandardPartItemBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
StandardPartItemBuilder
¶ Bases:
NXOpen.Builder
Represents the ship standard part item builder.
This class cannot be directly instantiated and has to be created by CreateStandardPartItem.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
FifthObject | Returns the fifth selected object. |
FirstAdoptionCurve | Returns the first adoption curve. |
FirstChainInstallDirection | Returns or sets the flag to indicate whether to flip the direction of the first selected chain object or not. |
FirstChainObject | Returns the first chain selected object. |
FirstObject | Returns the first selected object. |
FirstPlane | Returns the first selected plane. |
FourthObject | Returns the fourth selected object. |
InstallFifthDirection | Returns or sets the flag to indicate whether to flip the direction of the fifth selected object or not. |
InstallFirstDirection | Returns or sets the flag to indicate whether to flip the direction of the first selected object or not. |
InstallFourthDirection | Returns or sets the flag to indicate whether to flip the direction of the fourth selected object or not. |
InstallSecondDirection | Returns or sets the flag to indicate whether to flip the direction of the second selected object or not. |
InstallThirdDirection | Returns or sets the flag to indicate whether to flip the direction of the third selected object or not. |
SecondAdoptionCurve | Returns the second adoption curve. |
SecondChainInstallDirection | Returns or sets the flag to indicate whether to flip the direction of the second selected chain object or not. |
SecondChainObject | Returns the second chain selected object. |
SecondObject | Returns the second selected object. |
SecondPlane | Returns the second selected plane. |
Tag | Returns the Tag for this object. |
ThirdObject | Returns the third selected object. |
Methods¶
Method | Description |
---|---|
AddAcrossObject | Adds the specific object to the across object list. |
AddDeselectedAcrossObject | Adds the specific object to the deselected across object list. |
CheckScallopSize | Checks the scallop size by enabling the predefined requirement check inside the standard part, and resets to original state afterwards. |
Commit | Commits any edits that have been applied to the builder. |
ConvertReferenceGeometry | Converts the selected reference geometry. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
LookupRegistration | Checks the registration context string when an object is selected. |
RemoveAcrossObject | Removes the specific object from the across object list. |
RemoveDeselectedAcrossObject | Removes the specific object from the deselected across object list. |
ResetItem | Resets the standard part item builder to its intial state. |
SetOptionalGeometry | Sets one geometry for input selection which has multiple options. |
SetTransitionGeometry | Sets the transition geometry given the index. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateReferences | Updates and relinks the external references. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StandardPartItemBuilderDirection Enumeration | Represents the ship standard part installation direction and thickness direction. |
Property Detail¶
FifthObject¶
-
StandardPartItemBuilder.
FifthObject
¶ Returns the fifth selected object.
-------------------------------------
Getter Method
Signature
FifthObject()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: None.
FirstAdoptionCurve¶
-
StandardPartItemBuilder.
FirstAdoptionCurve
¶ Returns the first adoption curve.
-------------------------------------
Getter Method
Signature
FirstAdoptionCurve()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.2.
License requirements: None.
FirstChainInstallDirection¶
-
StandardPartItemBuilder.
FirstChainInstallDirection
¶ Returns or sets the flag to indicate whether to flip the direction of the first selected chain object or not.
-------------------------------------
Getter Method
Signature
FirstChainInstallDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstChainInstallDirection(firstChainInstallDirection)
Parameters: firstChainInstallDirection ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
FirstChainObject¶
-
StandardPartItemBuilder.
FirstChainObject
¶ Returns the first chain selected object.
-------------------------------------
Getter Method
Signature
FirstChainObject()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
FirstObject¶
-
StandardPartItemBuilder.
FirstObject
¶ Returns the first selected object.
-------------------------------------
Getter Method
Signature
FirstObject()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: None.
FirstPlane¶
-
StandardPartItemBuilder.
FirstPlane
¶ Returns the first selected plane.
-------------------------------------
Getter Method
Signature
FirstPlane()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: None.
FourthObject¶
-
StandardPartItemBuilder.
FourthObject
¶ Returns the fourth selected object.
-------------------------------------
Getter Method
Signature
FourthObject()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: None.
InstallFifthDirection¶
-
StandardPartItemBuilder.
InstallFifthDirection
¶ Returns or sets the flag to indicate whether to flip the direction of the fifth selected object or not.
-------------------------------------
Getter Method
Signature
InstallFifthDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InstallFifthDirection(fifthDirectionInstall)
Parameters: fifthDirectionInstall ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
InstallFirstDirection¶
-
StandardPartItemBuilder.
InstallFirstDirection
¶ Returns or sets the flag to indicate whether to flip the direction of the first selected object or not.
-------------------------------------
Getter Method
Signature
InstallFirstDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InstallFirstDirection(firstDirectionInstall)
Parameters: firstDirectionInstall ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
InstallFourthDirection¶
-
StandardPartItemBuilder.
InstallFourthDirection
¶ Returns or sets the flag to indicate whether to flip the direction of the fourth selected object or not.
-------------------------------------
Getter Method
Signature
InstallFourthDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InstallFourthDirection(fourthDirectionInstall)
Parameters: fourthDirectionInstall ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
InstallSecondDirection¶
-
StandardPartItemBuilder.
InstallSecondDirection
¶ Returns or sets the flag to indicate whether to flip the direction of the second selected object or not.
-------------------------------------
Getter Method
Signature
InstallSecondDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InstallSecondDirection(secondDirectionInstall)
Parameters: secondDirectionInstall ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
InstallThirdDirection¶
-
StandardPartItemBuilder.
InstallThirdDirection
¶ Returns or sets the flag to indicate whether to flip the direction of the third selected object or not.
-------------------------------------
Getter Method
Signature
InstallThirdDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InstallThirdDirection(thirdDirectionInstall)
Parameters: thirdDirectionInstall ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SecondAdoptionCurve¶
-
StandardPartItemBuilder.
SecondAdoptionCurve
¶ Returns the second adoption curve.
-------------------------------------
Getter Method
Signature
SecondAdoptionCurve()
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.2.
License requirements: None.
SecondChainInstallDirection¶
-
StandardPartItemBuilder.
SecondChainInstallDirection
¶ Returns or sets the flag to indicate whether to flip the direction of the second selected chain object or not.
-------------------------------------
Getter Method
Signature
SecondChainInstallDirection()
Returns: Return type: NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondChainInstallDirection(secondChainInstallDirection)
Parameters: secondChainInstallDirection ( NXOpen.Features.ShipDesign.StandardPartItemBuilderDirection
) –New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SecondChainObject¶
-
StandardPartItemBuilder.
SecondChainObject
¶ Returns the second chain selected object.
-------------------------------------
Getter Method
Signature
SecondChainObject()
Returns: Return type: NXOpen.ScCollector
New in version NX8.0.0.
License requirements: None.
SecondObject¶
-
StandardPartItemBuilder.
SecondObject
¶ Returns the second selected object.
-------------------------------------
Getter Method
Signature
SecondObject()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: None.
SecondPlane¶
-
StandardPartItemBuilder.
SecondPlane
¶ Returns the second selected plane.
-------------------------------------
Getter Method
Signature
SecondPlane()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: None.
ThirdObject¶
-
StandardPartItemBuilder.
ThirdObject
¶ Returns the third selected object.
-------------------------------------
Getter Method
Signature
ThirdObject()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX8.0.0.
License requirements: None.
Method Detail¶
AddAcrossObject¶
-
StandardPartItemBuilder.
AddAcrossObject
¶ Adds the specific object to the across object list.
Signature
AddAcrossObject(acrossObject)
Parameters: acrossObject ( NXOpen.DisplayableObject
) – body, face or curve entity.New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
AddDeselectedAcrossObject¶
-
StandardPartItemBuilder.
AddDeselectedAcrossObject
¶ Adds the specific object to the deselected across object list.
Signature
AddDeselectedAcrossObject(acrossObject)
Parameters: acrossObject ( NXOpen.DisplayableObject
) – body, face or curve.New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
CheckScallopSize¶
-
StandardPartItemBuilder.
CheckScallopSize
¶ Checks the scallop size by enabling the predefined requirement check inside the standard part, and resets to original state afterwards.
If there is no vialation of the requirement, nothing will happen.
Signature
CheckScallopSize()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ConvertReferenceGeometry¶
-
StandardPartItemBuilder.
ConvertReferenceGeometry
¶ Converts the selected reference geometry.
For instance stiffener curve, which represents stiffener body, into an equivalent reference geometry such as molding face, opposing molding face, top face.
Signature
ConvertReferenceGeometry(index, selObj)
Parameters: - index (int) –
- selObj (
NXOpen.DisplayableObject
) –
New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
LookupRegistration¶
-
StandardPartItemBuilder.
LookupRegistration
¶ Checks the registration context string when an object is selected.
Signature
LookupRegistration()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
RemoveAcrossObject¶
-
StandardPartItemBuilder.
RemoveAcrossObject
¶ Removes the specific object from the across object list.
Signature
RemoveAcrossObject(acrossObject)
Parameters: acrossObject ( NXOpen.DisplayableObject
) – body, face or curve.New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
RemoveDeselectedAcrossObject¶
-
StandardPartItemBuilder.
RemoveDeselectedAcrossObject
¶ Removes the specific object from the deselected across object list.
Signature
RemoveDeselectedAcrossObject(acrossObject)
Parameters: acrossObject ( NXOpen.DisplayableObject
) – body, face or curve.New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
ResetItem¶
-
StandardPartItemBuilder.
ResetItem
¶ Resets the standard part item builder to its intial state.
Signature
ResetItem()
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SetOptionalGeometry¶
-
StandardPartItemBuilder.
SetOptionalGeometry
¶ Sets one geometry for input selection which has multiple options.
Multiple options could come from selection configuration setting, or several geometries with the same attributes.
Signature
SetOptionalGeometry(selectedGeometry)
Parameters: selectedGeometry ( NXOpen.DisplayableObject
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
SetTransitionGeometry¶
-
StandardPartItemBuilder.
SetTransitionGeometry
¶ Sets the transition geometry given the index.
Signature
SetTransitionGeometry(index, transitionGeometry)
Parameters: - index (int) –
- transitionGeometry (
NXOpen.DisplayableObject
) –
New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
UpdateReferences¶
-
StandardPartItemBuilder.
UpdateReferences
¶ Updates and relinks the external references.
bToUpdateGeometry is used to decide if the input geometries need to be recalculated.
Signature
UpdateReferences(bToUpdateGeometry)
Parameters: bToUpdateGeometry (bool) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_basic (“Ship Basic Design”)
Validate¶
-
StandardPartItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.