StandardPartFrameworkBuilderSmartRuleStage Enumeration¶
NXOpen.Features.ShipDesign.StandardPartFrameworkBuilder.SmartRuleStage is an alias for NXOpen.Features.ShipDesign.StandardPartFrameworkBuilderSmartRuleStage
-
class
NXOpen.Features.ShipDesign.
StandardPartFrameworkBuilderSmartRuleStage
¶ Bases:
object
Indicates the stage of the smart rule.
Enum Members
Enum Member Enum Member Description PreUpdate In pre-update stagePostUpdate In post-update stage-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-