SplitProfilePlateBuilderToolOptionType Enumeration¶
NXOpen.Features.ShipDesign.SplitProfilePlateBuilder.ToolOptionType is an alias for NXOpen.Features.ShipDesign.SplitProfilePlateBuilderToolOptionType
-
class
NXOpen.Features.ShipDesign.
SplitProfilePlateBuilderToolOptionType
¶ Bases:
object
Represents trim tool type to trim profile or plate solid body.
Enum Members
Enum Member Enum Member Description Plane Select existed datum or face for the tool target.NewPlane Create a new datum for the tool target.Extrude Select curve and direction as extrude for the tool target.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-