SplitProfilePlateBuilderSplitDirectionOptionType Enumeration¶
NXOpen.Features.ShipDesign.SplitProfilePlateBuilder.SplitDirectionOptionType is an alias for NXOpen.Features.ShipDesign.SplitProfilePlateBuilderSplitDirectionOptionType
-
class
NXOpen.Features.ShipDesign.
SplitProfilePlateBuilderSplitDirectionOptionType
¶ Bases:
object
Represents split direction to trim profile or plate solid body .
Enum Members
Enum Member Enum Member Description PerpendicularToMoldingFace create plane/face perpendicular to molding face as the split toolAlongPlaneOrFace Split profile/plate along selected plane or face-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-