ShipnameFieldBuilderType Enumeration¶
-
class
NXOpen.Features.ShipDesign.
ShipnameFieldBuilderType
¶ Bases:
object
Field Type Enum Members
Enum Member Enum Member Description Fixed Field with an unchanging stringOption Field whose value can be one of several stringsIndex Field which will have a number generatedAny Field whose value will be a user enterred stringPositionInformation Field which is generated from mold face plane indicate part locationContextAttributeMap Field whose value comes from context attributeSectionType Field whose value comes from sub section typeNotSet Unknown Field Type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-