ShipPreparationInfoTypes Enumeration¶
NXOpen.Features.ShipDesign.ShipPreparationInfo.Types is an alias for NXOpen.Features.ShipDesign.ShipPreparationInfoTypes
-
class
NXOpen.Features.ShipDesign.
ShipPreparationInfoTypes
¶ Bases:
object
Used to specify the type of object represented in the data.
Enum Members
- when needed. “
- “EdgeReinforcementEdges”, ” The data represents a edge reinforcement divide feature. This feature handles labelling the edges
- of the linked body. “
- “StandardPartBracketDivide”, ” The data represents a standard part bracket divide feature. ” “Pillar”, ” The data represents a pillar feature. ” “BracketDivide”, ” The data represents a bracket divide feature. ” “UserDefined”, ” The data represents a user defined divide feature. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.