ShipEndCutBuilderCreationMethod Enumeration¶
NXOpen.Features.ShipDesign.ShipEndCutBuilder.CreationMethod is an alias for NXOpen.Features.ShipDesign.ShipEndCutBuilderCreationMethod
-
class
NXOpen.Features.ShipDesign.
ShipEndCutBuilderCreationMethod
¶ Bases:
object
available methods used to place a cutout object
Enum Members
Enum Member Enum Member Description FaceEdge 1 face and 1 edge are used to place this endcutSpecifyCSYS a csys is used to place this endcut-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-