ShipDesignPreferencesBuilderTypes Enumeration¶
NXOpen.Features.ShipDesign.ShipDesignPreferencesBuilder.Types is an alias for NXOpen.Features.ShipDesign.ShipDesignPreferencesBuilderTypes
-
class
NXOpen.Features.ShipDesign.
ShipDesignPreferencesBuilderTypes
¶ Bases:
object
This enum represents the ship structure types.
Enum Members
Enum Member Enum Member Description Hull Hull typeDeck Deck typeTransverseBulkhead Transverse Bulkhead typeLongitudinalBulkhead Longitudinal Bulkhead typeGenericPlateSystem Generic Plate System typeStiffenerSystem Stiffener System typeEdgeReinforcementSystem Edge Reinforcement System typePillarSystem Pillar System typeScantlingSeam Scantling Seam typeErectionSeam Erection Seam typeStrakingSeam Straking Seam typeIntersectionSeam Intersection Seam typeBracket Bracket typeCollarPlate Collar Plate type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-