ShipDesignPreferencesBuilderAngleRuleTypes Enumeration¶
NXOpen.Features.ShipDesign.ShipDesignPreferencesBuilder.AngleRuleTypes is an alias for NXOpen.Features.ShipDesign.ShipDesignPreferencesBuilderAngleRuleTypes
-
class
NXOpen.Features.ShipDesign.
ShipDesignPreferencesBuilderAngleRuleTypes
¶ Bases:
object
The methods that can be used to measure angles in ship design.
Enum Members
Enum Member Enum Member Description RightHand Angle is measured using the right hand rule system.ShipOrientation Angle direction and reference position is determined by the location in the ship.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-