ShipCoordinatesBuilderSelection Enumeration¶
NXOpen.Features.ShipDesign.ShipCoordinatesBuilder.Selection is an alias for NXOpen.Features.ShipDesign.ShipCoordinatesBuilderSelection
-
class
NXOpen.Features.ShipDesign.
ShipCoordinatesBuilderSelection
¶ Bases:
object
Represents the options to select point or component.
Enum Members
Enum Member Enum Member Description Point Allows point selection.Component Allows routing component selection.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-