ShipAttributeHolder Class¶
-
class
NXOpen.Features.ShipDesign.
ShipAttributeHolder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Features.ShipDesign.ShipAttributeHolder
builderThis is an abstract class.
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CopyAttributesToObjects | Copies attributes from proxy to feature objects |
CopyAttributesToPart | Copies the attributes to part |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAttributeProxy | Gets attribute proxy @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAttributeToProxyFromBuilder | Sets attribute proxy |
SetAttributesToObjects | Sets the attributes to feature objects |
SetAttributesToProxy | Sets the attributes to proxy |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
CopyAttributesToObjects¶
-
ShipAttributeHolder.
CopyAttributesToObjects
¶ Copies attributes from proxy to feature objects
Signature
CopyAttributesToObjects(bCreate, featBuilder)
Parameters: - bCreate (bool) – create or edit
- featBuilder (
NXOpen.Features.FeatureBuilder
) –
New in version NX8.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
CopyAttributesToPart¶
-
ShipAttributeHolder.
CopyAttributesToPart
¶ Overloaded method CopyAttributesToPart
CopyAttributesToPart(object)
CopyAttributesToPart(bCreate, featBuilder)
-------------------------------------
Copies the attributes to part
Signature
CopyAttributesToPart(object)
Parameters: object (list of NXOpen.NXObject
) –New in version NX8.0.0.
Deprecated since version NX8.0.1: This method is no longer valid. Use the un-deprecated method with the same method name.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
-------------------------------------
Copies the attributes from proxy to part
Signature
CopyAttributesToPart(bCreate, featBuilder)
Parameters: - bCreate (bool) – create or edit
- featBuilder (
NXOpen.Features.FeatureBuilder
) –
New in version NX8.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
-------------------------------------
GetAttributeProxy¶
-
ShipAttributeHolder.
GetAttributeProxy
¶ Gets attribute proxy
Signature
GetAttributeProxy()
Returns: Return type: NXOpen.NXObject
New in version NX8.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
SetAttributeToProxyFromBuilder¶
-
ShipAttributeHolder.
SetAttributeToProxyFromBuilder
¶ Sets attribute proxy
Signature
SetAttributeToProxyFromBuilder(featBuilder)
Parameters: featBuilder ( NXOpen.Features.FeatureBuilder
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
SetAttributesToObjects¶
-
ShipAttributeHolder.
SetAttributesToObjects
¶ Overloaded method SetAttributesToObjects
SetAttributesToObjects(object)
SetAttributesToObjects(bCreate, featBuilder)
-------------------------------------
Sets the attributes to feature objects
Signature
SetAttributesToObjects(object)
Parameters: object (list of NXOpen.NXObject
) –New in version NX8.0.0.
Deprecated since version NX8.0.1: Use
NXOpen.Features.ShipDesign.ShipAttributeHolder.SetAttributesToProxy()
instead.License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
-------------------------------------
Sets the attributes to objects
Signature
SetAttributesToObjects(bCreate, featBuilder)
Parameters: - bCreate (bool) – create or edit
- featBuilder (
NXOpen.Features.FeatureBuilder
) –
New in version NX8.0.1.
Deprecated since version NX8.0.2: Use
NXOpen.Features.ShipDesign.ShipAttributeHolder.SetAttributesToProxy()
instead.License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
-------------------------------------
SetAttributesToProxy¶
-
ShipAttributeHolder.
SetAttributesToProxy
¶ Sets the attributes to proxy
Signature
SetAttributesToProxy(object)
Parameters: object ( NXOpen.NXObject
) – NULL or object to be editedNew in version NX8.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”) OR nx_ship_mfg_prep (“Ship Manufacturing”)
Validate¶
-
ShipAttributeHolder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.