ShellTemplateBuilderTypes Enumeration¶
NXOpen.Features.ShipDesign.ShellTemplateBuilder.Types is an alias for NXOpen.Features.ShipDesign.ShellTemplateBuilderTypes
-
class
NXOpen.Features.ShipDesign.
ShellTemplateBuilderTypes
¶ Bases:
object
The option for controlling how the coordinate system for template creation is specified.
Enum Members
Enum Member Enum Member Description Manual Manually specify the coordinate system.InferCoordinateSystem Derive the coordinate system.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-