ShellTemplateBuilderPlaneLocationTypes Enumeration¶
NXOpen.Features.ShipDesign.ShellTemplateBuilder.PlaneLocationTypes is an alias for NXOpen.Features.ShipDesign.ShellTemplateBuilderPlaneLocationTypes
-
class
NXOpen.Features.ShipDesign.
ShellTemplateBuilderPlaneLocationTypes
¶ Bases:
object
The option for how the plane locations will be specified as input.
Enum Members
Enum Member Enum Member Description Existing Use existing planes to define the individual template locations.Offset Derive the plane locations from the orientation coordinate system or X and Y specified base planes-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-