SectionViewBuilderSymmetricalStructureOptions Enumeration¶
NXOpen.Features.ShipDesign.SectionViewBuilder.SymmetricalStructureOptions is an alias for NXOpen.Features.ShipDesign.SectionViewBuilderSymmetricalStructureOptions
-
class
NXOpen.Features.ShipDesign.
SectionViewBuilderSymmetricalStructureOptions
¶ Bases:
object
Settings to indicate to show symmetrical structure
Enum Members
Enum Member Enum Member Description Full Show full section view of the bulkheadPort Only show port side of the bulkhead section view. Starboard Only show starboard side of the bulkhead section view.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-