SectionDrawingBuilderViewTypeOptions Enumeration¶
NXOpen.Features.ShipDesign.SectionDrawingBuilder.ViewTypeOptions is an alias for NXOpen.Features.ShipDesign.SectionDrawingBuilderViewTypeOptions
-
class
NXOpen.Features.ShipDesign.
SectionDrawingBuilderViewTypeOptions
¶ Bases:
object
Settings to indicate the view type.
Enum Members
Enum Member Enum Member Description BasicDesign the view is created on basic designDetailDesign the view is created on detail design-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-